i.MX6DuaLite, Machine name?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DuaLite, Machine name?

823 Views
mahaiyang
Contributor II

I hava a board named EPC6708, the processor is i.MX6DuaLite.

Freescale Public GIT 

Which name do I choose(fsl-arm-yocto-bsp.git or meta-fsl-bsp-release.git or other)?
Corresponding machine name?

Tags (1)
0 Kudos
Reply
2 Replies

692 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi ma haiyang,

For instance you may use imx6dlsabresd because the kernel would be the same, but please note that the hardware configuration would be different in your board than in imx6dlsabresd. So you need to change the Device Tree file and use onde that describes your hardware.

I did something similar with the UDOO board where I used imx6qsabresd MCHINE. Please take a look here:

Building Linux Image with QT5 for UDOO Quad 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

692 Views
mahaiyang
Contributor II

Thanks for your answer.

Best Regards.

0 Kudos
Reply