i.MX6DuaLite, Machine name?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6DuaLite, Machine name?

712 次查看
mahaiyang
Contributor II

I hava a board named EPC6708, the processor is i.MX6DuaLite.

Freescale Public GIT 

Which name do I choose(fsl-arm-yocto-bsp.git or meta-fsl-bsp-release.git or other)?
Corresponding machine name?

标记 (1)
0 项奖励
回复
2 回复数

581 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi ma haiyang,

For instance you may use imx6dlsabresd because the kernel would be the same, but please note that the hardware configuration would be different in your board than in imx6dlsabresd. So you need to change the Device Tree file and use onde that describes your hardware.

I did something similar with the UDOO board where I used imx6qsabresd MCHINE. Please take a look here:

Building Linux Image with QT5 for UDOO Quad 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

581 次查看
mahaiyang
Contributor II

Thanks for your answer.

Best Regards.

0 项奖励
回复