i.MX6DQ Android Beam animation issue.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DQ Android Beam animation issue.

ソリューションへジャンプ
3,038件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ Android BSP.

When use Android Beam with jb4.2.2_1.0.0, a animation works on the background.

If repeat this animation, android will freeze and reboot without any log.

And if disable watchdog, the issue will be only freeze and reboot is not occurred.

On the other hand, this issue is resolved by jb4.2.2_1.1.0.

So we think some patch resolves this issue, and we want to know what patch do it.

Could you let me know what patch file resolves it?

Best Regards,

Satoshi Shimoda

ラベル(3)
0 件の賞賛
返信
1 解決策
2,810件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

It appears to be an issue with the GPU driver.  Is there a reason for not moving to 4.2.2.1.1 ?

You can try the GPU driver from 4.2.2.1.1 in 4.2.2.1.0 (attached).


You can find jb4.2.2_1.1.0 GPU user space binaries in attach, please apply them on your board.

There are five GPU patches in kernel, you can find them in attach, please apply them to jb4.2.2_1.0.0 kernel and re-build the boot.img.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,811件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

It appears to be an issue with the GPU driver.  Is there a reason for not moving to 4.2.2.1.1 ?

You can try the GPU driver from 4.2.2.1.1 in 4.2.2.1.0 (attached).


You can find jb4.2.2_1.1.0 GPU user space binaries in attach, please apply them on your board.

There are five GPU patches in kernel, you can find them in attach, please apply them to jb4.2.2_1.0.0 kernel and re-build the boot.img.

0 件の賞賛
返信
2,810件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

SergioSolis, can you please comment?

0 件の賞賛
返信
2,810件の閲覧回数
YixingKong
Senior Contributor IV

SergioSolis, could you help in following the request, or do you need help from others?

Thanks,

Yixing

0 件の賞賛
返信
2,810件の閲覧回数
YixingKong
Senior Contributor IV

SergioSolis, could you help in following the request, or do you need help from others?

Thanks,

Yixing

0 件の賞賛
返信
2,810件の閲覧回数
satoshishimoda
Senior Contributor I

Could you let me know your status?

I would appreciate if you send me a reply as soon as possible.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信