i.MX6DL LVDS clock issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DL LVDS clock issue

3,859 Views
j_wolters
Contributor I

Hello,

I'm trying to connect a 10.3 LVDS display with 1920x720 resolution. Unfortunately the display stays black. When measuring the display clock it doesn's goes higher then 50mhz instead of configured 89mhz.

I Modified the Device Tree Files like this:

&clks {
  fsl,ldb-di0-parent = <&clks IMX6QDL_CLK_PLL2_PFD0_352M>;
  fsl,ldb-di1-parent = <&clks IMX6QDL_CLK_PLL2_PFD0_352M>; 
};
&ldb { status = "okay"; lvds-channel@0 { reg = <0>; fsl,data-mapping = "spwg"; fsl,data-width = <24>; status = "okay"; primary; display-timings { native-mode = <&timing0>; timing0: 1920x720 { clock-frequency = <89000000>; hactive = <1920>; vactive = <720>; hback-porch = <0>; hfront-porch = <0>; vback-porch = <0>; vfront-porch = <0>; hsync-len = <112>; vsync-len = <10>; pixelclk-active = <0>; }; }; }; }; Thanks in advance, Jordan
Labels (2)
0 Kudos
Reply
4 Replies

3,681 Views
j_wolters
Contributor I

Issue is fixed by changing the "clks" in dtb file.

&clks {
      fsl,ldb-di0-parent = <&clks IMX6QDL_CLK_PLL2_PFD0_352M>;
      fsl,ldb-di1-parent = <&clks IMX6QDL_CLK_PLL2_PFD0_352M>; 
};

to:

&clks {

        assigned-clocks = <&clks IMX6QDL_CLK_LDB_DI0_SEL>, <&clks IMX6QDL_CLK_LDB_DI1_SEL>;

        assigned-clock-parents = <&clks IMX6QDL_CLK_PLL2_PFD0_352M>, <&clks IMX6QDL_CLK_PLL2_PFD0_352M>; 

};

0 Kudos
Reply

3,681 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jordan

one can look at various lcd examples for different resolutions on boundary boards

linux-imx6/imx6qdl-nitrogen6_max.dtsi at boundary-imx_4.9.x_8mq_ga-pass1-ath10k · boundarydevices/li... 

Configuring i.MX6 boards for different screens - Boundary Devices 

Also single channel supports up to 85 MHz (WXGA 1366x768@60)
for bigger resolutions split mode should be used as described in
Table 40-5. Channel Mapping i.MX6SDL Reference Manual
http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,681 Views
j_wolters
Contributor I

Hi Igor,

Thanks for your reply. I have display working with correct display clock currently. 

Unfortunately this is with an old yocto and kernel version. For now it works on Yocto 2.1.2 (krogoth) with kernel 4.1.15, but the same dts configuration doesn't work with Yocto 2.5.2 (sumo) and kernel 4.9.88.

Can there be some different lvds configurations in kernel?

Best regard,

Jordan

0 Kudos
Reply

3,681 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jordan

nxp support sumo only starting with L4.14.78 :

linux-imx - i.MX Linux kernel 

For L4.9.88 rocko is used according to Linux 4.9.88_2.0.0 BSP & Multimedia Codecs Documentation

Best regards
igor

0 Kudos
Reply