Hi
We are able to do firmware update using mfgtool on custom board.
We are getting error like "Block device MMC2 not supported".
booti mmc2
MMC detect: 1
CMD_SEND:0
ARG 0x00000000
MMC_RSP_NONE
CMD_SEND:8
ARG 0x000001AA
MMC_RSP_R1,5,6,7 0x00000000
CMD_SEND:55
ARG 0x00000000
MMC_RSP_R1,5,6,7 0x00000000
** Block device MMC 2 not supported
Thanks
Saurabh
解決済! 解決策の投稿を見る。
Hi igor,
Finally I am able to get eMMC working.
We need to do GPIO correction in u-boot code.
Thanks for your support.
Saurabh
Hi Saurabh
seems card does not respond to reset (CMD_SEND:0),
except that one uses wrong mmc number,
smth basically wrong with mmc, please check power supplies
and signals with oscilloscope, one can do that with SDK test usdhc.c, running it with jtag
for mmc connections one can look at Sabre schematic
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
We can detect MMC when we boot from SD Card.
So it seems that power supply should be proper.
But u-boot code fails to detect eMMC.
is there any update available for eMMC in u-boot?
Thanks
Saurabh
Hi igor,
Finally I am able to get eMMC working.
We need to do GPIO correction in u-boot code.
Thanks for your support.
Saurabh