i.MX6D custom board boot from eMMC failes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6D custom board boot from eMMC failes

ソリューションへジャンプ
1,626件の閲覧回数
saurabh206
Senior Contributor III

Hi

We are able to do firmware update using mfgtool on custom board.

We are getting error like "Block device MMC2 not supported".

booti mmc2

MMC detect: 1

CMD_SEND:0

                ARG                      0x00000000

                MMC_RSP_NONE

CMD_SEND:8

                ARG                      0x000001AA

                MMC_RSP_R1,5,6,7         0x00000000

CMD_SEND:55

                ARG                      0x00000000

                MMC_RSP_R1,5,6,7         0x00000000

** Block device MMC 2 not supported

Thanks

Saurabh

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,376件の閲覧回数
saurabh206
Senior Contributor III

Hi igor,

Finally I am able to get eMMC working.

We need to do GPIO correction in u-boot code.

Thanks for your support.

Saurabh

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,376件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Saurabh

seems card does not respond to reset (CMD_SEND:0),

except that one uses wrong mmc number,

smth basically wrong with mmc, please check power supplies

and signals with oscilloscope, one can do that with SDK test usdhc.c, running it with jtag

i.MX 6Series Platform SDK

for mmc connections one can look at Sabre schematic

i.MX6_SABRE_SDP_DESIGNFILES

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,376件の閲覧回数
saurabh206
Senior Contributor III

Hi igor,

We can detect MMC when we boot from SD Card.

So it seems that power supply should be proper.

But u-boot code fails to detect eMMC.

is there any update available for eMMC in u-boot?

Thanks

Saurabh

0 件の賞賛
返信
1,377件の閲覧回数
saurabh206
Senior Contributor III

Hi igor,

Finally I am able to get eMMC working.

We need to do GPIO correction in u-boot code.

Thanks for your support.

Saurabh

0 件の賞賛
返信