i.MX6D USB ENVADJ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6D USB ENVADJ

1,622件の閲覧回数
sugiyamatoshihi
Contributor V

Hi, 

I'd like to know the tolerance of ENVADJ voltage. Also, what is voltage source of ENVADJ?

The ENVADJ field adjusts the trip point for the envelope detector.
000 = Trip-Level Voltage is 0.12500 V
001 = Trip-Level Voltage is 0.10000 V
010 = Trip-Level Voltage is 0.13750 V
011 = Trip-Level Voltage is 0.15000 V
1XX = Reserved

Best Regards,

Sugiyama

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,494件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Toshishisa,

    The voltage setting is used to set the trip point for the envelope detector, and evelope detector will determine if the current usb signal on differential line is valid  according to the voltage.


Have a great day,
TIC  weidong sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,494件の閲覧回数
sugiyamatoshihi
Contributor V

Hi, weidong sun,

Thank you for the answer.

However, I'd like to know below items of ENVADJ voltage.

1. How this voltage generate in circuit?  From USB LDO?

2. How much the voltage vary by each device?   When 000=125mV, does the voltage vary +/-5mV?

3. How much the voltage vary depend on temperature?  About 35degC, the voltage seems minimum.

Best Regards,

Sugiyama

0 件の賞賛
返信

1,494件の閲覧回数
sugiyamatoshihi
Contributor V

Hi, 

Could you answer?

Best Regards,

Sugiyama

0 件の賞賛
返信