I use android_M6.0.1_2.0.0_source BSP to develop my product.
Android: android-6.0.1_r22
Kernel: Linux/arm 4.1.15
The kernel config file is ".config"
The log message is "log2.txt"
In this enviornment, linux kernel will run to dead.
When I use "Linux/arm 3.14.52 Kernel" will no this problem.
Original Attachment has been moved to: .config.zip
Original Attachment has been moved to: log2.txt.zip
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Aress
there are no specific errors related to security, so this may be
caused by build or programming issues. Please try fresh build
and program using MFG Tools
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Aress
unfortunately there is no such support for Android secure boot as for LInux,
suggest to elevate this through local fae channel.
Best regards
igor
Hi Igor,
Thanks for your reply and suggestion. I will retry another way.
Best regards,
Aress.