i.MX6 internal thermal sensor safe values

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 internal thermal sensor safe values

1,257 Views
himanshu_gupta
Contributor I

Hello,

What is the actual location of i.MX6 internal thermal sensor ? How the temperature values are different from Tj. What are the recommended safe limits of temperature to throttle down the frequency or shutdown the processor?

0 Kudos
Reply
1 Reply

1,037 Views
igorpadykov
NXP Employee
NXP Employee

Hi Himanshu

thermal sensor is described on app notes :

AN5215 i.MX 6 Temperature Sensor Module
http://www.nxp.com/docs/en/application-note/AN5215.pdf
AN4579 i.MX 6 Series Thermal Management Guidelines
http://cache.nxp.com/docs/en/application-note/AN4579.pdf

Actual location of i.MX6 internal thermal sensor is not available,

one can consider that it measures Tj.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply