i.MX6 SoloX maximum RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 SoloX maximum RAM

2,678 Views
peder_alm
Contributor I

1. What is the maximum amount of RAM that I can use for the i.MX6 SoloX? 1GB?

2. Where in the datasheet can I get this information?

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

2,505 Views
karangajjar
Senior Contributor II

Hi Peder Alm 

Please refer Table 2-2. CM4 memory map in IMX6SXRM.pdf. In that you can see MMDC x32DDR Controller which shows the maximum RAM for cortex M-4.

Let us know in case of any concerns.

 

Regards,

Karan Gajjar

0 Kudos
Reply

2,505 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Peter,

DDR Controller supports 16/32-bit LPDDR2-800, DDR3-800 and DDR3L-800. The maximum RAM that the MX6SX can support is given in Table 2-1. System memory map i.MX6SX Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6SXRM.pdf

2GB for Cortex-A9 and 1.5GB for Cortex-M4

0 Kudos
Reply

2,505 Views
peder_alm
Contributor I

I found the reference for 2GB for Cortex-A9 (MMDC), but where do I find it for the Cortex-M4 in the table?

memory_map.png

0 Kudos
Reply