i.MX6 SPI clocking

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 SPI clocking

2,807 Views
davidmüller
Contributor I

Hello

As far as i can see, the i.MX6 ECSPI controller starts clocking after the CS goes low and stops before CS goes high. Unfortunately this seems to confuse some SPI devices. Is there a (undocumented) way to configure the ECSPI controller to start clocking before the CS goes low or to provide a continuous clock?

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

2,274 Views
terrykelleher
Contributor I

This is the way SPI is supposed to operate. SCLK is ignored by a SPI Slave unless the SS# is asserted. Starting the clock early would have no good impact, and might cause issues if the first falling edge occurs coincidentally with the falling SS#.

I cannot imagine you would be able to take over the SCLK with GPIO, as the SPI Master needs to insure that data is ready prior to the falling clock edge. An independent clock would be out of sync.

Terry

0 Kudos
Reply

2,274 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

you can use GPIO as CS,

there are no other undocumented settings, all are given in RM.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,274 Views
davidmüller
Contributor I

Thanks for your fast answer but I think I would rather need to set up the CLK line as GPIO to achieve a running clock before CS goes low. Unfortunately this contradicts the concept of having a dedicated SPI controller hardware.:smileysad:

0 Kudos
Reply