i.MX6 SATA-II

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 SATA-II

2,306件の閲覧回数
wanglee
Contributor III

        我做了一个兼容iMX6D和iMX6Q的板卡,但是我发现iMX6D(MCIMX6D5EYM10AC-QCD1602)不支持SATA-II,但是iMX6Q支持,我觉得我的硬件是没有问题的。但是按照官方的说明,iMX6D应该是支持SATA-II的,这是为什么?

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,911件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Q: [Translated by Google]: I made a compatible iMX6D and iMX6Q board, but I found iMX6D
(MCIMX6D5EYM10AC-QCD1602) does not support SATA-II, but iMX6Q support,
I think my hardware is no problem. However, according to the official note, iMX6D
should support SATA-II, which is why?

A: iMX6D has the same SATA module as iMX6Q and it also supports SATA-II.

Please try to adjust sata signal shape described in sect.36.4.14 GPR (IOMUXC_GPR13)

i.MX6DQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

May be recommended to perform sata eye pattern test:

https://community.nxp.com/message/975623?commentID=975623#comment-975623 

Best regards
igor

0 件の賞賛
返信

1,911件の閲覧回数
wanglee
Contributor III

The power level  in  SATA_VP pin  is higher (1.28V) than normol (1.1V), how to  lower the power level to normal? will  this  degrade  the performance or destroy the IC ?

0 件の賞賛
返信