i.MX6 Processor Schematic symbol

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Processor Schematic symbol

1,451件の閲覧回数
muralikrishna
Contributor I


Hi,

We are using MCIMX6Q6AVT10AD processor in our design.

we are OrCAD16.6 Software for creating the Schematics.

Is the processor symbol is available for preparing the schematics?

Kindly advise

ラベル(1)
0 件の賞賛
返信
1 返信

1,282件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

My recommendation would be to download the Schematic files for Freescale’s Reference Boards, opening the Schematics and then exporting the processor symbol. It might not be very straightforward but there is no symbol library available on Freescale’s website.

The symbol would be the same for all i.MX6Q processors as the differences between part numbers are related to temperature, certification or clock frequency, so you should be covered using the symbol from the i.MX&Q SABRE Board.

0 件の賞賛
返信