i.MX6 - Kernel changes for 2GB RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 - Kernel changes for 2GB RAM

1,548 Views
Ansari
Contributor IV

Dear sir/Madam,

We are using i.MX6Q custom board based on sabreSD board and we are using Linux-3.10.17_1.0.0-GA BSP for our development.

We have upgraded the RAM size into 2GB (earlier it was 1GB).

We would like to know the changes required in u-boot and Kernel for 2GB with below BSPs.

1. Linux-3.10.17_1.0.0-GA

2. L3.0.35_4.1.0_130816

Regards,

Ansari

0 Kudos
Reply
1 Reply

1,387 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to  Chapter 1 (Porting U-Boot from an i.MX 6 Reference

Board to an i.MX 6 Custom Board) of “i.MX_BSP_Porting_Guide.pdf” in

FSL Linux documentation.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply