i.MX6 IPUx_DI0_STAT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 IPUx_DI0_STAT

2,366 次查看
sugiyamatoshihi
Contributor V

Hi, 

I have questions about function of IPUx_DI10_STAT register of IPU in i.MX6DQ reference manual. 

1. There are status bits of DI0_CNTR_FIFO_FULL and  DI0_READ_CNTR_EMPTY.

    What FIFO status does it indicate?  Does this FIFO use data transfer from DMFC/Memory to DI0?

2. There are status bits of DI0_READ_FIFO_FULL and DI0_READ_FIFO_EMPTY.

   What FIFO status does it indicate?  Does this FIFO use data transfer from smart Display or DMFC/Frame buffer?

Best Regards,

Sugiyama

标签 (1)
0 项奖励
回复
5 回复数

2,173 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sugiyama

>Does it means DI0_CNTR_FIFO is for output data to parallel display?

yes

Best regards
igor

0 项奖励
回复

2,173 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sugiyama

>1. There are status bits of DI0_CNTR_FIFO_FULL and  DI0_READ_CNTR_EMPTY.
>    What FIFO status does it indicate?  

This FIFO is part of the DI0 synchronizer, depicted on Figure 37-39 DI's block diagram
i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

>Does this FIFO use data transfer from DMFC/Memory to DI0?

No. DMFC has not direct connection to DI0, as shown on p.33 "IPUv3H – Internal Structure"
presentation on
https://community.nxp.com/docs/DOC-100482 

 
>2. There are status bits of DI0_READ_FIFO_FULL and DI0_READ_FIFO_EMPTY.
>   What FIFO status does it indicate?  

This FIFO is part of the DI0 synchronizer, depicted on Figure 37-39 DI's block diagram.

>Does this FIFO use data transfer from smart Display or DMFC/Frame buffer?

It i used for smart display, not supported in i.MX6 IPU.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,173 次查看
sugiyamatoshihi
Contributor V

Hi, Igor,

Thank you for the answer.

There are two synchronizer in Fig 37-39. 

 Does  DI0_CNTR_FIFO_  refer to DC's Data Accumulater and clock domain Synchronizer?

If so, is it possible that this FIFO status detect data error sent from DC? 

Does DI0_READ_FIFO refer to Parallel Interface Data Synchronizer?

Best Regards,

Sugiyama

0 项奖励
回复

2,173 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sugiyama

>There are two synchronizer in Fig 37-39.
>Does  DI0_CNTR_FIFO_  refer to DC's Data Accumulater and clock domain Synchronizer?

it refers to Parallel Interface Data Synchronizer

>Does DI0_READ_FIFO refer to Parallel Interface Data Synchronizer?

yes

Best regards
igor

0 项奖励
回复

2,173 次查看
sugiyamatoshihi
Contributor V

Hi, Igor,

Thank you for the answer.

Does it means DI0_CNTR_FIFO is for output data to parallel display?

Best Regards,

Sugiyama

0 项奖励
回复