i.MX6 ECSPI CS & timing issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 ECSPI CS & timing issues

3,725 Views
juliencorjon
Contributor I

Dear All,

I'm facing several issues with communication between an i.MX6Q ECSPI2 and an FPGA. Goal is to write 8bits address and read a 32bits value as fast as we can.

In my DTS file I set-up ECSPI2 to use SCLK/MISO/MOSI/SS0 and I wrote my own fpga kernel driver (kernel rel_imx_3.14.52_1.1.0_ga is compiled with imx-spi driver). You can find both at the end of this post.

First, here is a capture of two SPI transfert in one SPI message :

scope_6.png

Issue 1 : CS have to stay enabled between 8bits address writing and 32bits value reading.

Even if I set explicitely cs_change to 0 in my kernel driver, CS is disabled between the two bursts. I assume that I have to set SS_CTL to 0 but I have no idea how to do that in my driver

Note : If I change CS from SS0(DISP0_DAT18 - ALT2) to GPIO5_IO12 (DISP0_DAT18 - ALT5) this CS issue disappear - see oscilloscope print bellow - but I'd prefer to use native ECSPI CS.

scope_7.png

Issue 2 : Why Is there a CLK tick between the two SPI message?

This issue is the same than the one describe here : https://community.nxp.com/message/625531#comment-625531 but solution have not been found yet.

Issue 3 : Time to take / release SPI communication is huge

As you can notice in the oscilloscope prints the time to take / release the SPI communication is really disappointing. I assume this is because SPI communication is handled by the kernel instead of the ECSPI bloc. Is there any way to change that?

Issue 4 : How to handle a 40bits SPI message with BURST ECSPI capability in my FPGA kernel driver?

-------------------------------------------------------------

=== DTS File ===

&ecspi2 {

  pinctrl-names = "default";

  pinctrl-0 = <&pinctrl_ecspi2>;

  fsl,spi-num-chipselects = <1>;

  cs-gpios = <0>;

  status = "okay";

  fpga: fpga {

  compatible = "eca,fpga";

  reg = <0>;

  spi-max-frequency = <20000000>;

  };

};

&iomuxc {

  ecspi2 {

  pinctrl_ecspi2: ecspi2grp {

  fsl,pins = <

  MX6QDL_PAD_DISP0_DAT17__ECSPI2_MISO 0x100b1

  MX6QDL_PAD_DISP0_DAT16__ECSPI2_MOSI 0x100b1

  MX6QDL_PAD_DISP0_DAT19__ECSPI2_SCLK 0x100b1

  MX6QDL_PAD_DISP0_DAT18__ECSPI2_SS0  0x100b1

  >;

                };

  };

}

=== SPI driver ===

static int eca_fpga_reg_read(void *context, unsigned int reg, unsigned int *out)

{

  struct device *dev = context;

  struct spi_transfer t[2];

  struct spi_message m;

  u8 address;

  __le32 val;

  int ret;

  mutex_lock(&spi_lock);

  address = (reg << 1) | 0x1;

  spi_message_init(&m);

  memset(t, 0, sizeof(t));

  t[0].tx_buf = &address;

  t[0].len = sizeof(address);

  t[0].cs_change = 0;

  t[0].bits_per_word = 8;

  t[1].rx_buf = &val;

  t[1].len = sizeof(val);

  t[1].bits_per_word = 32;

  spi_message_add_tail(&t[0], &m);

  spi_message_add_tail(&t[1], &m);

  ret = spi_sync(to_spi_device(dev), &m);

  mutex_unlock(&spi_lock);

  if (ret)

  return ret;

  *out = cpu_to_le32(val);

  return 0;

}

Any advice/hint/solution is more than welcome :smileyhappy:

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,220 Views
igorpadykov
NXP Employee
NXP Employee

Hi Julien

1. "cs_change" is not used in nxp ecspi driver (please check attached

Linux Manual Chapter 37) and sources/dts documentation :

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/Documentation/devicetree/bindings/s...

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/drivers/spi/spi-imx.c?h=imx_3.14.52...

In general one can add support for it using "of_get_named_gpio" in  spi_imx_probe()

function. To avoid CS disabling between the two bursts it is necessary to set ECSPIx_CONREG

BURST_LENGTH with data burst and provide algorithm to avoid emptying TX FIFO, untill

all bits data sent out.

2. issue was not confirmed by nxp expert, in particular one can pay attention to

ERR009606 eCSPI: In master mode, burst lengths of 32n+1 will transmit incorrect data

3. timing may be affected by OS overheads, so one can try to optimize it removing

unused modules and tasks with heavy graphic.

4. set ECSPIx_CONREG[BURST_LENGTH] for 40 data burst and provide such algorithm

so TX FIFO was never empty, untill all data sent.

Note, NXP has service for helping customers with porting drivers:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Pro-Support contact www.nxp.com/prosupport

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply