i.MX6_Boot Mode setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6_Boot Mode setting

2,951件の閲覧回数
jackyc_wu
Contributor I

Hi, 
I have some board bring up issue, Need help for setting Boot Config. 
The MPU is i.MX6ull, chosen SD card and eMMC for my boot device ,Reference document :IMX6ULLRM Rev. 0, 09/2016 

Issue as below : 

RM Section 5 - 
SD/eSD Boot Fusemap (Table 5-5) 
1. BOOT_CFG1 [0] : What is SD Loopback Clock Source Sel ? through SD pad and direct means ? 
2. BOOT_CFG1 [1] : Is SD POWER Cycle Enable means that if i had RST pin with my boot deviece, choose -> Enabled via USDHC_RST pad ? if not, choose No power cycle? 
3. BOOT_CFG1 [3:2] : How to choose ? any suggestion ? 
4. BOOT_CFG1 [4] : Is SDR25 SDR50 SDR104 -> Fast Boot? if not, why? 
5. BOOT_CFG2 [7:6] : What is SD Calibration Step means, and how to setting ? 

MMC/eMMC Boot Fusemap (Table 5-6) 
6. BOOT_CFG1[0] : Same problem as the 1st point 
7. BOOT_CFG1[1] : Same problem as the 2nd point 
8. BOOT_CFG1[3:2] : What is Fast Boot Acknowledge Disable setting depends and its meaning ? 
What version of eMMC will it be high speed mode or Regular? 

Please help, and extremely grateful! 
Best regards, 

Jacky.

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,613件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 You may create request to get boot utility to review boot log.

Regards,

Yuri.

0 件の賞賛
返信

2,614件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Jack,

About the boot mode settting you can refer to the i.MX6ULL schematic boot up design. You can directly refer to it. And in your case you created our engineer have give reply to you, please have a check.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信