i.MX6 APE codec

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 APE codec

2,418件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I want to ask how to decode the APE file.

Customer want to play the file encoded with APE.

It seems that the Linux 4.1.15 does not include APE codec.

 

Q1.

Could you tell us the solution to play the APE file on i.MX6 series L 4.1.15?

 

Best Regards,

 

0 件の賞賛
返信
1 返信

2,171件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

please refer to attached Release Notes sect.6 Multimedia

for supported codecs in official nxp bsps. Support for other codecs

may be provided as software codec. One can seek support on developers site

Monkey's Audio - a fast and powerful lossless audio compressor 

and other linux opensource resources.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信