i.MX53 SABRE Tablet: Getting Linux Penguin, but not the Android Screen

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX53 SABRE Tablet: Getting Linux Penguin, but not the Android Screen

4,816 次查看
dn
Fresh Out Contributor

I am having a problem not getting the Android screen when the target boots up.  I get the Linux penguin on the tablet screen, but that's it.  I don't get the Android screen afterwards. The Android shell works on the serial port.  I built the Android image according to i.MX Android R10.4 User Guide.  I am booting up from SD card.

 

I don't get this problem when I run the prepackage binaries from the image_imx-android-r10.4_53smd folder.  The Android screen shows up after the Linux penguin screen. 

 

Has anyone had the problem?  Is there startup script that I have to configure?

标签 (1)
标记 (2)
0 项奖励
回复
4 回复数

4,254 次查看
visakh
Contributor III

is your  load address and uboot recognition is correct?.... is there any error in ramdisk loading? if so, you replace your uRamdisk.img with the prebuilt and try....then figure out

0 项奖励
回复

4,254 次查看
JayZhang
Fresh Out Contributor

Dear,

Is that the cross compile toolchain?

I think you can check the log between your build image and packaged image, can you show me?

Is there any android log? init.rd file that corret?

0 项奖励
回复

4,254 次查看
dn
Fresh Out Contributor

I am using the same boot arguments in uboot for both my build and the prepackaged binaries, but the outcome is different.  I figure that is something wrong with my build, because the prepackaged binaries run fine.

0 项奖励
回复

4,254 次查看
JayZhang
Fresh Out Contributor

Hi,

You'd better check the boot argument in uboot.

0 项奖励
回复