i.MX53 QSB-R with WEC7 and Android sample binaries from Adeneo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 QSB-R with WEC7 and Android sample binaries from Adeneo

1,848 Views
StuartBoutell
Contributor I

Anyone else having trouble with the sample WEC7 and Android binaries from Adeneo on the i.MX53 QSB-R revision? I understand the PMIC has changed on the QSB-R versus QSB.

 

Android boots, but then shuts down into a powersaving state, with USB not appearing to operate and there is a kernel message about the PMIC revision during the boot up

pmic 0-0008: read generation ID 0x0 is not equal to 0x7!

 

WEC7 (iMX53QSB_WEC7_BIN_V122) doesn't boot at all, stopping with this error (from eboot in this case, but the nk image does the same):

OALPmicI2cInit: Trying to init PMIC I2C Interface
OALPmicInit: Trying to init I2C Interface
OALI2CReadOneByte: OALI2cWriteData Set Reg Error!
OALPmicInit: Read of PMIC hardware rev failed!
OEMPlatformInit: OALPmicInit failed!

Tags (1)
0 Kudos
Reply
1 Reply

1,655 Views
G_rio
Contributor III

Hello Freescale and Adeneo,

I have the same issue as above.

I'm trying to run it qith VGA video and iMX53QSB_WEC7_BIN_V122. How to fix it ?

INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb

BSP Clock Configuration:

    OSC         =   24000000 Hz

    PLL1        =  800000000 Hz

    PLL2        =  600000000 Hz

    PLL3        =  400000000 Hz

    PLL4        =  595000000 Hz

    LP_APM      =   24000000 Hz

    ARM         = 1000000000 Hz

    AXI_A       =  300000000 Hz

    AXI_B       =  200000000 Hz

    EMI_SLOW    =  120000000 Hz

    AHB         =  120000000 Hz

    IPG         =   60000000 Hz

    PERCLK      =    8000000 Hz

    CKIL_SYNC   =      32768 Hz

    DDR         =  300000000 Hz

    ARM_AXI     =  200000000 Hz

    IPU_HSP     =  200000000 Hz

    VPU_AXI     =  200000000 Hz

    GPU         =  200000000 Hz

    GPU2D       =  200000000 Hz

    DEBUG_APB   =  200000000 Hz

    ENFC        =   30000000 Hz

    USBOH3      =   66666666 Hz

    ESDHC1      =  100000000 Hz

    ESDHC2      =  100000000 Hz

    ESDHC3      =  100000000 Hz

    ESDHC4      =  100000000 Hz

    UART        =   24000000 Hz

    SSI1        =    6000000 Hz

    SSI2        =    6000000 Hz

    SSI3        =    6000000 Hz

    SSI_EXT1    =   24000000 Hz

    SSI_EXT2    =   19047619 Hz

    USB_PHY     =   24000000 Hz

    TVE_216_54  =  297500000 Hz

    DI0         =   50000000 Hz

    DI1         =  297500000 Hz

    VPU_RCLK    =   24000000 Hz

    SSI_LP_APM  =   24000000 Hz

    SPDIF_XTAL  =   24000000 Hz

    LDB_DIO     =  595000000 Hz

    LDB_DI1     =  595000000 Hz

    SPDIF0      =    1142857 Hz

    ESAI        =    3000000 Hz

    ESAI_HCKR   =          0 Hz

    ESAI_HCKT   =          0 Hz

    CAN         =   60000000 Hz

    FIRI        =   24000000 Hz

    CSI_MCLK1   =   25000000 Hz

    CSI_MCLK2   =   25000000 Hz

    ECSPI       =   66666666 Hz

    LPSR        =          0 Hz

    PGC         =    7500000 Hz

    ASRC        =   59500000 Hz

    IEEE_CEMX   =   40000000 Hz

    CKIH        =   22579200 Hz

    CKIH2       =          0 Hz

Microsoft Windows CE Bootloader Common Library Version 1.4 Built Aug 26 2011 10:39:37

OALPmicI2cInit: Trying to init PMIC I2C Interface

OALPmicInit: Trying to init I2C Interface

OALI2CReadOneByte: OALI2cWriteData Set Reg Error!

OALPmicInit: Read of PMIC hardware rev failed!

OEMPlatformInit: OALPmicInit failed!

0 Kudos
Reply