i.MX53 MACRO for eboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 MACRO for eboot

1,506 Views
chengwu
Contributor I

Dear all,

     I'm developing a wince7 BSP on an i.MX53 board, my board is boot from nand flash, so the nand driver would be used by both eboot and OS, but now I have some code in nand driver should be used only in eboot, so I want to use some macro to make those code out of build when I building the OS, are there any macros could distinguish which program is building(eboot or OS)? Or are there any macro & environment only available in eboot/OS?

Thank you very much.

Labels (1)
0 Kudos
Reply
1 Reply

1,436 Views
igorpadykov
NXP Employee
NXP Employee

Hi cheng

frankly speaking I am not aware of such macros.

In general NAND algorithms (and BBT in particular) are quite complex

to be implemeneted as macros.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply