i.MX53 IPU VDI Channel path

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 IPU VDI Channel path

2,438件の閲覧回数
cader
Contributor I

Dear all,

i.MX53 IPU supports many channel paths as mentioned below where VDI involves.
1. CSI –> VDI –> MEM
2. MEM –> VDI –> MEM
3. MEM –> VDI –> IC –> MEM
4. CSI –> VDI –> IC –> MEM
5. and so on.
 
We want to validate the second channel path (MEM –> VDI –> MEM ) mentioned above which is applicable for type of de-interlace application.
Please let us know MEM –> VDI –> MEM path is tested and if so, please provide the test application which just read from interlaced video file and outputs the de-interlaced video in another file.

Please share the idea or any one did the same.

Thanks in Advance.
Cader.

タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,078件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

Hi Cader, I think you can reference to vpu_unit_test code, which can be found in BSP unit test code.

The test application can do de-interlance in MEM->VDI->MEM(Frame buffer).

You can also reference to my blog: http://imxcommunity.org/profiles/blogs/1080i-de-interlance-support-for-imx53-based-on-l2-6-35-11-09-...

0 件の賞賛
返信

2,078件の閲覧回数
GaoJianzhong
Contributor IV

Hi Li Qiang,

I want to use

CSI –> VDI –> IC –> MEM, is there anything to reference?

should i need to modify the driver?

0 件の賞賛
返信

2,078件の閲覧回数
JianqingChen
Contributor II

Do you have solved the problem?I want to work on CSI->VDI->MEM.But it failed.In kernel_imx/drivers/media/video/mxc/capture/,there has CSI->PRP->MEM example.I modified it but no success.If you have any idea,please contact me.My email is [email protected]!

0 件の賞賛
返信