i.MX53 Cache Flush Using Set/Way

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 Cache Flush Using Set/Way

1,531件の閲覧回数
geseeker
Contributor I

Hi guys,

Is anyone aware of how to flush the L1/L2 d-cache for a particular physical address using the set and way method (using the c7 coprocessor)? More specifically, I'd like to know the mapping between a physical address and its corresponding set/way, so that the exact slot in the cache that needs to be flushed can be specified. The ARMARM says that this mapping is implementation defined, so I'm wondering what the imx53-specific mapping is.

I'm aware that there is another method to flush a particular entry in the cache, by specifying the MVA. However, we're currently experimenting with some monitoring code in the secure world (using the TrustZone extension) where MMU is disabled, so MVA wouldn't have much meaning and therefore doesn't work. We would like to flush a particular cache slot for the normal world so that we can apply the monitor code correctly.

タグ(2)
0 件の賞賛
返信
1 返信

1,429件の閲覧回数
JerryFan
NXP Employee
NXP Employee

I am not sure, but maybe you can try to convert the virtual address of the NS word the the virtual address of Secure word, and then do the flushing by MVA.

0 件の賞賛
返信