i.MX50: Pads for Muxed 16-bit NOR Flash boot mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX50: Pads for Muxed 16-bit NOR Flash boot mode

跳至解决方案
1,258 次查看
norishinozaki
Contributor V

Hello Champs

I set 00 in BOOT_CFG2[7:6] for muxed 16-bit NOR Flash boot, the data and address pins are connected to the pads in Yellow?

20677_20677.pngpastedImage_0.png

Best regards,

Nori Shinozaki

标签 (1)
0 项奖励
回复
1 解答
1,126 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,127 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
1,127 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nori

you are right: EIM_DA[15:0} are used for mode

BOOT_CFG2[7:6]=00  for muxed 16-bit NOR Flash boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复