Running Ubuntu on i.MX6 SDP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running Ubuntu on i.MX6 SDP

ソリューションへジャンプ
2,829件の閲覧回数
dmitryv
Contributor II

Hello!

I'm looking for a general procedure for running Ubuntu and OpenOffice on i.MX6 SDP.

I suppose that they can be added and built as a package or layer with Yocto, since Ubuntu looks like just a set of packages with their dependencies. Or is it much more complicated?

I know there is a pre-built image in download section. But it is built with older kernel and only suitable for SDP (and not suitable for custom board), so I think it is only for demo purposes. Is it correct?

Looking for a short guidance to understand what is possible and how complicated is it. Thank you!

--

Dmitry

ラベル(3)
0 件の賞賛
返信
1 解決策
2,631件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,632件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
2,631件の閲覧回数
Yuri
NXP Employee
NXP Employee

Dmitry, good day !


   Generally it is possible to configure i.MX6 board for I-net access and just run

$ sudo apt-get install ....

I did not try Open Office, but some other packages can be installed in such a way.

~Yuri.

0 件の賞賛
返信
2,631件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dmitry

regarding integration of OpenOffice I would suggest to

post this on meta-fsl-arm mailing list, so that someone familiar with Yocto/OpenOffice

could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

As for pre-built image in download section - yes it is built for

Freescale reference boards only and there is new yocto 3.10.17 image

L3.10.17_1.0.2_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo

Linux Binary Demo Files and Linux BSP Documentation.

Size (K): 717480 Format: gz Rev #: L3.10.17_1.0.2 Modified: 10/29/2014

L3.10.17_1.0.0_LINUX_DOCS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信