Hello Champs
I set 00 in BOOT_CFG2[7:6] for muxed 16-bit NOR Flash boot, the data and address pins are connected to the pads in Yellow?
Best regards,
Nori Shinozaki
Solved! Go to Solution.
Hi Nori
you are right: EIM_DA[15:0} are used for mode
BOOT_CFG2[7:6]=00 for muxed 16-bit NOR Flash boot
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------