i.MX50 EVK D4 LED

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,675件の閲覧回数
andrewstorus
Contributor I

Hello all,

I have been experiencing problems loading and running Ubuntu 10.04 from my i.MX50 EVK. Whenever the board is powered on, the red D4 led continuously blinks at a rate of about 3 per minute, while no video is output from the HDMI. I am assuming the blinking of the D4 led means no OS found, but have been unable to find documentation specifically pertaining to this. If anyone knows the meaning of this, it would be greatly appreciated.

Regards,
Andrew

ラベル(1)
0 件の賞賛
返信
1 解決策
2,550件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

per Err36 MC34708 Errata document (used in EVK):

"Charger function no longer supported"

http://cache.freescale.com/files/analog/doc/errata/MC34708ER.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,551件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

per Err36 MC34708 Errata document (used in EVK):

"Charger function no longer supported"

http://cache.freescale.com/files/analog/doc/errata/MC34708ER.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,550件の閲覧回数
andrewstorus
Contributor I

Thank you for your reply Igor

0 件の賞賛
返信
2,550件の閲覧回数
andrewstorus
Contributor I

After digging around in the documentation I was able to find this -

"The CHRGLEDR will be activated when standalone charging is started and will remain under control of the state machine. When charging is complete, the CHRGLEDR is disabled and the CHRGLEDG is activated: LEDR: Charging LEDG: Charge finished" as per the SCH-26721-D data sheet

Now I am wondering if anyone else has experienced issues with the board not charging, or an expectation as to how long it should take. My board has been charging for quite some time now

0 件の賞賛
返信