i.MX287 DDR2 options?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX287 DDR2 options?

Jump to solution
4,596 Views
nextleveltechn
Contributor II

Hello everyone, still a newbie here. Currently working with a hardware engineer for design a custom board similar to the i.MX28 EVK. I know there are a few options for DDR2, most of the known working DDR2 chips that would follow the same EVK DDR routing have EOL'd. I know I can contact every supplier for DDR chips, but they will obviously be slightly biased. IF everyone can post what they have used or known to work well in the past/currently it would be of great help!

This will give me some confidence and direction to help isolate and compare with vendors. Other memory chips this isn't as critical, but it seems that DDR with i.MX is very critical.

Thanks in advance!

Labels (1)
1 Solution
4,417 Views
art
NXP Employee
NXP Employee

Any JEDEC-compliant DDR2 chip can be used with i.MX28 series processors.


Have a great day,
Artur

View solution in original post

7 Replies
4,418 Views
art
NXP Employee
NXP Employee

Any JEDEC-compliant DDR2 chip can be used with i.MX28 series processors.


Have a great day,
Artur

4,417 Views
MartinHo
Contributor IV

I'm using 2x MT47H64M16HR

regards

Martin

4,417 Views
nextleveltechn
Contributor II

Thank you for the information Martin!

0 Kudos
Reply
4,417 Views
ask
Contributor III

Hi Tom,

In our design winbond W971GG6KB25I used.

4,417 Views
nextleveltechn
Contributor II

Thank you for the information!

0 Kudos
Reply
4,417 Views
igorpadykov
NXP Employee
NXP Employee

HI Tom

I know that  MT47h32m16, MT46H128M16, Winbond W971GG6JB

used in i.MX28 designs.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

4,417 Views
nextleveltechn
Contributor II

Thank you for the information Igor!

0 Kudos
Reply