i.MX287 DDR2 options?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX287 DDR2 options?

ソリューションへジャンプ
4,675件の閲覧回数
nextleveltechn
Contributor II

Hello everyone, still a newbie here. Currently working with a hardware engineer for design a custom board similar to the i.MX28 EVK. I know there are a few options for DDR2, most of the known working DDR2 chips that would follow the same EVK DDR routing have EOL'd. I know I can contact every supplier for DDR chips, but they will obviously be slightly biased. IF everyone can post what they have used or known to work well in the past/currently it would be of great help!

This will give me some confidence and direction to help isolate and compare with vendors. Other memory chips this isn't as critical, but it seems that DDR with i.MX is very critical.

Thanks in advance!

ラベル(1)
1 解決策
4,496件の閲覧回数
art
NXP Employee
NXP Employee

Any JEDEC-compliant DDR2 chip can be used with i.MX28 series processors.


Have a great day,
Artur

元の投稿で解決策を見る

7 返答(返信)
4,497件の閲覧回数
art
NXP Employee
NXP Employee

Any JEDEC-compliant DDR2 chip can be used with i.MX28 series processors.


Have a great day,
Artur

4,496件の閲覧回数
MartinHo
Contributor IV

I'm using 2x MT47H64M16HR

regards

Martin

4,496件の閲覧回数
nextleveltechn
Contributor II

Thank you for the information Martin!

0 件の賞賛
返信
4,496件の閲覧回数
ask
Contributor III

Hi Tom,

In our design winbond W971GG6KB25I used.

4,496件の閲覧回数
nextleveltechn
Contributor II

Thank you for the information!

0 件の賞賛
返信
4,496件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Tom

I know that  MT47h32m16, MT46H128M16, Winbond W971GG6JB

used in i.MX28 designs.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

4,496件の閲覧回数
nextleveltechn
Contributor II

Thank you for the information Igor!

0 件の賞賛
返信