i.MX285: Error Linux Multimedia Framework -blog archive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX285: Error Linux Multimedia Framework -blog archive

1,393件の閲覧回数
AlisonLuanLOHR
Contributor I

I copy the fsl-mm-codeclib-1.9.6.tar.gz and gst-fsl-plugin-1.9.6 inside ltib/rootfs/var/tmp/pkgs.

Inside the ltib configuration interface, i select the "gstreamer-fsl-plugin" in "Freescale Multimedia Plugins/Codecs and "gstreamer-plugin-good". This according to the Linux Multimedia Framework, page 9-13.

During the compilation i have this error:

 

Build path taken because: no prebuilt rpm,
Testing network connectivity
OK GPP:

Try fsl-mm-codeclib-1.9.6.tar.gz.md5 from the GPP
http://bitshrine.org/gpp/fsl-mm-codeclib-1.9.6.tar.gz.md5:
07:46:29 ERROR 404: Not Found.
Try fsl-mm-codeclib-1.9.6.tar.gz from the GPP
http://bitshrine.org/gpp/fsl-mm-codeclib-1.9.6.tar.gz:
07:46:30 ERROR 404: Not Found.
Can't get: fsl-mm-codeclib-1.9.6.tar.gz at ./ltib line 790.


f_buildrpms() returned an error, exiting
traceback:
main:560


Started: Thu Jun 9 07:46:05 2011
Ended: Thu Jun 9 07:46:30 2011
Elapsed: 25 seconds

These packages failed to build:
fsl-mm-codeclib

Build Failed

Exiting on error or interrupt

 

How can i solve this problem?

タグ(1)
0 件の賞賛
返信
1 返信

1,257件の閲覧回数
G_rio
Contributor III
Have you tried to put these files in /opt/freescale/pkgs ?
0 件の賞賛
返信