i.MX28 u-boot fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 u-boot fail

1,294 Views
JHY
Contributor IV

Hi, I use i.MX28 in a custom board and want to use only VDD5V power source.

After applying L2.6.35_10.12_5V_SUPPLY_PATCH, SPL runs without problems but u-boot loading is fail printing out consol messages 'Undefined Ins'.

3.3V, 1.8V, 1.5V outputs are good and memory access tests have no error in SPL, only u-boot loading has problems.

Futhermore when I use DCDC4P2 power source in same board, it works all right, SPL, u-boot, lnux and every apps.

Are there missing pieces?

The registers are below,

All of DCDC_ENABLE=DCDC_XFER=LINREG_OFFSET=DISABLE_FET=0 and ENABLE_LINREG=1

 

5vctrl  (2403F592),

dcdc4p2 (A000001F),

vddd    (00F00710),

vdda    (000F070C),

vddio   (00070406),

vddmem  (00000230)

 

 

Labels (1)
0 Kudos
Reply
1 Reply

1,169 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

uboot and patch PMU settings are given for i.MX28 EVK and

may differ for custom board, in general you can add debug printfs to code

(or run it with jtag ) to find out where error condition (or brownout) occured.

It is not possible to give beforehand these settings for custom board since

they may differ one board from another.

Best regards

igor

0 Kudos
Reply