Hi,
I have an imx27ads board which got some problems when I turned on the board
as below:
++... Read from 0x07ee0000-0x07f00000 at 0xc1fe0000: .
... Read from 0x07ed3000-0x07ed4000 at 0xc1fff000: .
PMIC ID: 0x0000009b [Rev: 3.3]
Ethernet FEC MAC address: is not set
Board Type: EVB [rev A] (external UART doesn't work)
Clock input: 27 MHz
Booting from [NOR flash]
[Warning] FEC not connect right PHY: ID=fc03fc
FEC: [ HALF_DUPLEX ] [ connected ] [ 10M bps ]:
WARNING[can_send]: MXC_FEC is busy for transmittinig
WARNING[can_send]: MXC_FEC is busy for transmittinig
WARNING[can_send]: MXC_FEC is busy for transmittinig
Does anyone has ideas?
thanks a lot.
Elren
What is your Redboot version? On MX27ADS the 200749 works fine.
Regards,
Fabio Estevam
Looks like you are using an incorrect bootloader.
Looking at your log we see that the Board type is "EVB". On my ADS I see "ADS".
Maybe this can give you some clue.
Regards,
Fabio Estevam