i.MX27 Redboot issue: MXC_FEC is busy for transmittinig

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX27 Redboot issue: MXC_FEC is busy for transmittinig

3,248件の閲覧回数
Elren
Contributor I

Hi,
 
I have an imx27ads board which got some problems when I turned on the board
as below:
 
++... Read from 0x07ee0000-0x07f00000 at 0xc1fe0000: .
... Read from 0x07ed3000-0x07ed4000 at 0xc1fff000: .
PMIC ID: 0x0000009b [Rev: 3.3]
Ethernet FEC MAC address: is not set
Board Type: EVB [rev A] (external UART doesn't work)
Clock input: 27 MHz
Booting from [NOR flash]
[Warning] FEC not connect right PHY: ID=fc03fc
FEC: [ HALF_DUPLEX ] [ connected ] [ 10M bps ]:
WARNING[can_send]: MXC_FEC is busy for transmittinig
WARNING[can_send]: MXC_FEC is busy for transmittinig
WARNING[can_send]: MXC_FEC is busy for transmittinig


Does anyone has ideas?
thanks a lot.

Elren

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,187件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

What is your Redboot version? On MX27ADS the 200749 works fine.

 

Regards,

 

Fabio Estevam

0 件の賞賛
返信

2,187件の閲覧回数
Elren
Contributor I
I tried it on MX27ADS 200749 already and it doesn't work.
0 件の賞賛
返信

2,187件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Looks like you are using an incorrect bootloader.

 

Looking at your log we see that the Board type is "EVB". On my ADS I see "ADS".

 

Maybe this can give you some clue.

 

Regards,

 

Fabio Estevam

0 件の賞賛
返信

2,187件の閲覧回数
Elren
Contributor I

Thanks for your reply.

 

But the bootloader which I downloaded is getted from the BSP.

(imx27_ads_20071219-rel3-ltib.iso -> redboot_200749.tar.gz) 

 

I think the bootloader should be work.

 

Regards,

Elren 

0 件の賞賛
返信