i.MX27 MfgTool and Bulk-IO driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX27 MfgTool and Bulk-IO driver

ソリューションへジャンプ
1,235件の閲覧回数
siwoolee
Contributor I

Hi.

I want to download firmware to i.MX27 custom board with MfgTool on the Win 7.

but I meet fail message when I connect usb cable to PC with i.MX27 OTG.

Is there any way to do?

Firstly, I really want to connect i.MX27 as a Bulk-IO device driver on the Win 7.

Best regards.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
985件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

There’s no any version of mfgtool can support MX27. I suggest that you can Use Virtual Machine in Win7 to install a WinXP then use ATK tools.

元の投稿で解決策を見る

3 返答(返信)
985件の閲覧回数
siwoolee
Contributor I

Thank you for your reply.

I've been using ATK tools on the Window XP PC. but I failed to run ATK tool on the Window 7 PC.

As you know, ATK tools need Window 2000 or XP platform. 

so, I want to make MfgTool downloading i.MX7 image on the Window 7 platform.

Firstly, I meet device driver issue on the Window 7 platform with i.MX27 download mode.

0 件の賞賛
返信
986件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

There’s no any version of mfgtool can support MX27. I suggest that you can Use Virtual Machine in Win7 to install a WinXP then use ATK tools.

985件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for imx27, why don't you use ATK tools?

i.MX27 Processors|Robust Security for Mobile|NXP 

youc an download ATK tools, which can download image to mx27 board. and install on the windows.

0 件の賞賛
返信