i.MX25: OSC32K_EXTAL VIH/VIL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX25: OSC32K_EXTAL VIH/VIL?

Jump to solution
1,773 Views
norishinozaki
Contributor V

Hello Champs,

My customer is using an external clock circuit for 32.768KHz.

There is a spec for that in the data sheet.

pastedImage_0.png

They are using a circuit meets the spec(VOH/VOL) above, however the voltage at OSC32K_EXTAL is 2.3V which is lower than 0.7*VDD=2.31V.

This drop is considered because the circuit is providing clock not only to i.MX257 but also to a FPGA.

Is 2.3V for OSC32K_EXTAL OK?

What are VIH and VIL specs for OSC32K_EXTAL?

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
Reply
1 Solution
1,614 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

Table 10 gives Vih/Vil for 32.768KHz

as Recommended External Reference Clock Specifications

1.jpg

~igor

View solution in original post

0 Kudos
Reply
10 Replies
1,614 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

if voltage supply of OSC32K_EXTAL = 2.3V, VINL=0.69 (max)

VINH=1.61V(min)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,614 Views
norishinozaki
Contributor V

Hello Igor,

Thanks, but 2.3V is measured at customer's board.

There is no mention of Vih/Vil for 32.768KHz in the datasheet.

I'd like to know the spec.

Best regards,

Nori Shinozaki

0 Kudos
Reply
1,615 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

Table 10 gives Vih/Vil for 32.768KHz

as Recommended External Reference Clock Specifications

1.jpg

~igor

0 Kudos
Reply
1,614 Views
norishinozaki
Contributor V

Hello Igor,

My customer reported that voltage of 32.768KHz at OSC32K_EXTAL is too low, so I took the capture with i.MX25 EVK.

Please take a look at the attached capture.

i.MX25_EVK_CKIL.jpg

It is just 900mV!

It's lower than Vih(0.7 x VDD).

Is it acceptable?

The below is a 24MHz capture of i.MX25 EVK.

i.MX25_EVK_CKIH.jpg

It's amplitude is 2.220V which is also lower than Vih

It seems like i.MX25 is absorbing lots of current inside.

Is there any way to stop i.MX25 absorbing like this?

Best regards,

Nori Shinozaki

0 Kudos
Reply
1,614 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

I believe you measured waveforms with crystal, not

with external clock. Provided answer was for external clock

levels.

Best regards

igor

0 Kudos
Reply
1,614 Views
norishinozaki
Contributor V

Hello Igor,

Yes, it was from crystal.

You mean,  using crystal. the 900mV at OSC32K_EXTAL is OK.

Using an external clock circuite, it must be over 2.31V

With that said, why do you think 3.3V from the external clock drops to 2.31V at OSC32K_EXTAL?

The customer thinks the possibility that i.MX25 absorbs the current inside.

Best regards,

Nori Shinozaki

0 Kudos
Reply
1,614 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

yes these data is for external clock,

OSC32K_EXTAL does not absorb signal.

In general one needs to use external clock generator

with sufficient drive capability.

Best regards

igor

0 Kudos
Reply
1,614 Views
norishinozaki
Contributor V

Igor,

Thanks, I will check the customer's external clock design.

Best regards,

Nori Shinozaki

0 Kudos
Reply
1,614 Views
norishinozaki
Contributor V

Hello Igor,

I found the power rail of OSC32K_EXTAL is DRYICE in Table 101.

pastedImage_1.png

So the Table 10 should be read as follows, right?

pastedImage_3.png

Best regards,

Nori Shinozaki

0 Kudos
Reply
1,614 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

yes, I think you are right

Best regards

igor

0 Kudos
Reply