i.MX25 CAN driver for Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX25 CAN driver for Linux

3,218件の閲覧回数
giorgio_nedudgi
Contributor I

Hello All! I'm trying to use the CAN interface of the processor mentioned in the subject under Linux. However, although the processor is supported in the mainline kernel, the CAN controller is not. I surveyed the INTERNET, but however, I did not find any usable information. Does anybody has some suggestions on the topic; The best way would be to patch the mainstream kernel somehow to support the Controller. Thank you in advance for any help!

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,401件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Take a look at: http://lwn.net/Articles/343573/

 

Or if you are using Freescale MX27 Linux BSP there is FlexCAN support in  

rpm/BUILD/linux/drivers/net/can/flexcan

 

Regards,

 

Fabio Estevam

0 件の賞賛
返信

2,401件の閲覧回数
giorgio_nedudgi
Contributor I
Thank you, seems very usable, however I could not have a try right now. Anyway, I have a development board which has a factory linux which supports it's CAN controller. Could anybody give me a hint how to configure the the speed of the network from linux? Thank you very much in advance.
0 件の賞賛
返信