i.MX25 3-Stack board WinCE BSP PWM Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX25 3-Stack board WinCE BSP PWM Problem

1,669件の閲覧回数
zhoulishan
Contributor I

I use WinCE BSP with the i.MX25 3-Stack board.

The PWM used to drive the backlight on the i.MX25 3-Stack board is the PWM function within LCD Controller

instead of the PWM referenced in Chapter 37 of i.MX25 Reference Manual.

As the frequency of PWM within LCD Controller is too high(200KHz) or too low(110Hz) (We need 300Hz).

We use the PWM referenced in Chapter 37 of i.MX25 Reference Manual. We Set the PWM output frequency with

200Hz, used IPG_CLK32K as the source clock, it work prefect. But when We Set the GPIO3 GPIO[19] output high,

the PWM output a Waveform with random Duty. The registers of PWM seems set right (See Below), Can Anyone help

me ?

INFO: PWM REG Value

CR : 00030001

SR : 00000001

IR : 00000000

SAR: 0000001e

PR : 000000a0

CNR: 00000000


GPIO3_GPIO[19]--->IOMUXC_SW_MUX_CTL_PAD_POWER_FAIL = 0xb0

GPIO3_GPIO[19]--->IOMUXC_SW_MUX_CTL_PIN_POWER_FAIL = 0x05

PWM1--->IOMUXC_SW_MUX_CTL_PAD_PWM = 0xa0

PWM1--->IOMUXC_SW_MUX_CTL_PIN_PWM = 0x0

PWM4--->IOMUXC_SW_MUX_CTL_PAD_CONTRAST = 0xc0

PWM4->IOMUXC_SW_MUX_CTL_PIN_CONTRAST = 0x4

ラベル(2)
0 件の賞賛
返信
1 返信

1,447件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

The PWM driver enables the 3-Stack System to provide the following software and hardware support:

  1. 1. Supports duty cycle modulation
  2. 2. Supports varying output intervals
  3. 3. Supports two power management modes, full on and full off

The PWM driver outputs the toggling signal whose frequency and duty cycle can be modulated by programming the appropriate registers, please check your correct configuration for the IOMUX, The i.MX25 platform contains four PWM modules. PWM1 is conflicted with the interrupt from the Debug board. Therefore, this PWM can be used if the Debug board is not attached. PWM2 is used for USB OTG. PWM3 is used for USB OTG. PWM4 is conflicted with the LCD and CAN

Information about Wince Usage and unit test code please check the MX25 Wince BSP reference manual.

Regards