i.MX233 Board not powering up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX233 Board not powering up

915 Views
GopiNagaBharath
Contributor IV

Hello,

I have a custom board designed based on the i.MX23 CPU. When I powered the Battery input with 3.7V, the VDDXTAL is not giving out 1V. Since the VDDXTAL is source for turning ON the board with PSWITCH, I am unable to get the voltage on any other rails. Since the PMIC is internal and OFF, none of the power supply rails are active.

We have already designed i.MX23 based custom board which was working properly. This is a new design (with small changes from previous version) which is having this issue.

What are the reasons for the VDDXTAL not going to 1V (it is always 0V) ? I have probed the crystals, they too seem to be not powered and there is no clock.

Regards,

Gopi

Tags (1)
0 Kudos
Reply
2 Replies

783 Views
YixingKong
Senior Contributor IV

Gopi Naga

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

783 Views
YixingKong
Senior Contributor IV

Gopi Naga

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply