i.MX SoloLite / SLL: eInk Compatibility, Firmware, EoL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX SoloLite / SLL: eInk Compatibility, Firmware, EoL

跳至解决方案
1,882 次查看
ekerebel
Contributor III

Hello,

I am planning on using the i.MX 6 SoloLite for a navigation tablet that my team is designing. I have several questions:

- is the i.MX SoloLite compatible with both Carta 1.2 and Pearl?

- Does NXP provide the EPD firmware for any eInk panel (Carta 1.2 or Pearl)?

- Is there a scheduled End-of-Life for the 6 SoloLite?

- knowing that the tablet will not be using Ethernet, is there an advantage in considering the SLL (consumption?)

Erwan

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
1,797 次查看
b36401
NXP Employee
NXP Employee

Both i.MX6SL and i.MX6SLL processors have Electrophoretic Display Controller (EPDC) that supports displays up to 4096 x 4096 pixels.
You can refer to chapter 21 of i.MX6SL Reference Manual and chapter 19 of i.MX6SLL RM for the details.

i.MX6SL was launched in Nov 2012 and has 10 year longevity.
i.MX6SLL was launched in Jun 2017, so it will be produced at least till 2032.

One can refer i.MX 6SLL Power Consumption Measurement:
https://www.nxp.com/docs/en/application-note/AN12001.pdf

There is nothing special to i.MXSLL in point of Ethernet.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,798 次查看
b36401
NXP Employee
NXP Employee

Both i.MX6SL and i.MX6SLL processors have Electrophoretic Display Controller (EPDC) that supports displays up to 4096 x 4096 pixels.
You can refer to chapter 21 of i.MX6SL Reference Manual and chapter 19 of i.MX6SLL RM for the details.

i.MX6SL was launched in Nov 2012 and has 10 year longevity.
i.MX6SLL was launched in Jun 2017, so it will be produced at least till 2032.

One can refer i.MX 6SLL Power Consumption Measurement:
https://www.nxp.com/docs/en/application-note/AN12001.pdf

There is nothing special to i.MXSLL in point of Ethernet.

0 项奖励
回复