i.MX Keypad no device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Keypad no device

1,453件の閲覧回数
Mark78
Contributor I

Hallo,

I have activated the keypad driver in the kernel and configured the column and row keypads in the board file.

However, in the device filesystem is no entry /dev/input/input0.

I have started debugging and see that the function "imx_keypad_init" is called to register the function pointer for probing and remove, but the function "imx_keypad_probe" is never called.

Has somebody an idea what could be the reason?

THX

ラベル(1)
0 件の賞賛
返信
1 返信

1,348件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

What board are you using and which BSP?

Alejandro

0 件の賞賛
返信