I discussed with the AE team, please refer to the following update.
On i.MX 95, resource ownership and TRDC permissions are defined statically at build time in the SM config (mx95evk.cfg → generated config_.h) and applied by the System Manager (SM) when a MIX powers up. *There is no SCMI/SM message that transfers ownership of a peripheral from one Logical Machine (LM) to another at runtime.
However, SM documentation names "handing a display over from one LM to another" as the exact motivating use case for the SM_SCMI_PERM_EXCLUSIVE model. So the handover is achievable, just not by "moving" ownership.
Q1 & Q2 — MIPI DSI M7 → A55 handover: how to do it
The LMM (Logical Machine Management) SCMI protocol only boots / resets / shuts down / suspends / wakes LMs — it has no RESOURCE_ASSIGN or OWNERSHIP_TRANSFER message. Instead, use a temporal-division handoff:
- Grant BOTH LMs access up-front in mx95evk.cfg. By default the EVK config assigns MIPI_DSI, MIPI_PHY, DC_DISPENG, BLK_CTRL_DISPLAYMIX, the display clocks/power (PD_DISPLAY, CLK_DISP*) as OWNER of the AP (LM2) only — you must also add them to the M7 LM (LM1) to allow M7-first usage.
- Mark the SM-managed resources (clocks, power, reset) as SM_SCMI_PERM_EXCLUSIVE (api=all) so requests from the two LMs are not silently aggregated/overwritten.
- At handover, M7 quiesces DSI/DCIF, then signals A55 via application-level IPC (MU mailbox or SCMI notification). A55 (Linux/DRM DSI+DPU stack) then brings up the same IP.
The handoff sequencing is the customer's software responsibility (temporal division). The SM only guarantees the HW is drivable from either side because both LMs were pre-granted access. TRDC ownership cannot be rewritten at runtime — only the SM programs TRDC, and only from the static config at MIX power-up.
TRDC config that controls this (expressed in the .cfg):
- MDAC_am=… — Master-Domain Assignment (maps a bus master to a domain ID)
- MBC_am=s.b — Memory Block Check — this is where peripheral access is gated
- MRC_am=… — Memory Region Check (large memory regions like DDR)
- Each LM binds to a DID, e.g. SM did=2, AP(LM2) did=3, M7(LM1) did=4.
Q3 — Shared GPIO between M7 and A55
Yes, TRDC can grant both the M7 domain and the A55 domain concurrent access to the same GPIO instance (enable its MBC block for both DIDs). But there is a critical caveat and two supported patterns:
- Caveat: i.MX 95 GPIO has no hardware arbitration — PDR/DR/GDIR registers are physically shared, so uncoordinated read-modify-write from both cores races.
- Pattern A (disjoint pins + SW sync): Assign specific pins to each core by convention (the config already splits pins per LM). Since the data/direction register banks are still shared, protect concurrent RMW with a hardware semaphore / MU, or ensure the cores never touch the same register bank concurrently.
- Pattern B (SM-arbitrated, recommended for truly shared instances): Route through the always-on GPIO1, which is owned by the SM and whose documented role is "arbitrates shared access." IOMUXC/IOMUX_GPR are likewise SM-arbitrated. Pinmux/daisy is set via the SCMI pin-control protocol with per-agent permissions; GPIO data ops are direct MMIO.