i.MX 8X Ethernet Frame Parser Match Array table depth?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8X Ethernet Frame Parser Match Array table depth?

1,771 Views
andrelabelle111
Contributor I

Hi,

I have question about the i.MX 8XDualPlus Ethernet Frame Parser.

The reference manual describes the MAXINDEX field in ENET_RXPCTL as "Number of valid entries in the Match Array table." with a note saying the depth of the table is chip-specific. 

(i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual, Rev. D, 11/2018) page 3709

What is the depth of Match Array table?

Thanks.

Andre

0 Kudos
Reply
2 Replies

1,552 Views
indan_zupancic
Contributor I

My own tests show that the maximum is 64 entries (for the imx8qxp).

0 Kudos
Reply

1,720 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Andre,

I’m afraid that the i.MX8X is still on preproduction, so, no additional information could be provided yet. If you need assistance, please contact your Sales/FAE.

Best regards!

/Carlos

0 Kudos
Reply