i.MX 8QXP camera not accessible after adding ubuntu-rootfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8QXP camera not accessible after adding ubuntu-rootfs

1,538 Views
nolan_zinn
Contributor IV

I just finished following the procedure described at Build Ubuntu For i.MX8 Series Platform  to add Ubuntu on top of the Yocto rootfs (using Ubuntu-i.MX8-weston.pdf).  However, after making these changes, I no longer have access to my ov5640 camera module.  At boot time, I interrupt the boot and use 'setenv fdt_file fsl-imx8qxp-mek-ov5640-rpmsg.dtb' to load the correct device tree for the camera module.  Before adding Ubuntu, the camera was always at /dev/video4.  Let me know if there's any system info needed to diagnose the problem.  Thanks!

Tags (2)
0 Kudos
Reply
1 Reply

1,404 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, i.MX8QX is still in pre-production the BSP and the whole support may be subject to change. What I suggest you go with your DFAE. He could help you with this problem. I apologize for the inconvenience this may cause you.

Best regards,

Diego.

0 Kudos
Reply