Hi,
There is a 4GB DDR4 on my board, then I do the DDR stress test, region 2 is failed, it could not go to t0.2. However, it is ok if I set the device information as same as the MEK board, which means it is ok when I tested as 3GB DDR4. Could someone give me some advices please? Thanks.
The log is:
*************************************************************************
MX8 DDR Stress Test Version: ER14
Built on Mar 27 2020 12:28:23
*************************************************************************
--Set up the MMU and enable I and D cache--
- This is the Cortex-A35 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug
- VMCR Check:
- ttbr0_el3: 0x13d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x101122
- MMU and cache setup complete
*************************************************************************
ARM Clock(CA35): 1200MHz
DDR Clock: 1200MHz
============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 16, col size: 10
Two chip selects are used
Number of DDR controllers used on the SoC: 1
Density per chip select: 2048MB
Density per controller is: 4096MB
Total density detected on the board is: 4096MB
Command Bus Training was executed
No DDR data training errors detected for DDRC0
============================================
MX8QXP: Cortex-A35 is found
*************************************************************************
DDR Stress Test Iteration 1
--------------------------------
--Running DDR test on region 1--
--------------------------------
t0.1: data is addr test
....
t0.2: row hop read test
...
t1: memcpy SSN armv8_x32 test
....
t2: byte-wise SSN armv8_x32 test
..
t3: memcpy pseudo random pattern test
....................................................................
t4: IRAM_to_DDRv1 test
...
t5: IRAM_to_DDRv2 test
--------------------------------
--Running DDR test on region2--
--------------------------------
t0.1: data is addr test
...
Hi carolyn_zhang
one can check that latest RPA tool was used and versions of
RPA tool, SCFW and kernel were aligned to each other as described on below link
Best regards
igor
Totally speaking, I don't like the new community, it always show 'Article or Comment Not Found'.
Hi, Igorpadykov,
Thanks for your reply, but the website is useless since community changed a new revision. However, I have solved this problem by modified SCFW.
Thank you all the same.
Hi,
The default setting of SCFW is 3GB, change it to 4GB, rebuild SCFW and change scfw_download.bin in ddr_strss_test.