i.MX.8QM - Android Automotive 12 Audio Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX.8QM - Android Automotive 12 Audio Problem

1,705件の閲覧回数
kisstajmi
Contributor I

I Have an i.MX.8QuadMax processor with 88W8997 WIFI&BT module
and I have built a mek_8q_car-userdebug build
from Android Automotive 12.0.0_1.1.0 (Linux 8.10.72 Kernel)

The Problem is:
When I try to play built-in notification sound it works correctly. When I try to play built-in ringtones or I try to play music from a BT connected device or try to make/accept calls there is no any audible sound.

I tried it with multiple headphones & speakers (mono&stereo)

I assume it is an OS bug so how can I fix it?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,686件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @kisstajmi 

Please refer the 8.2 Audio configuration to route the audio sink:

https://www.nxp.com/docs/en/user-guide/Android_Auto_User's_Guide.pdf

0 件の賞賛
返信

1,656件の閲覧回数
kisstajmi
Contributor I

Thank you but in the 12.0.0.1 version the Android Auto User's Guide is not up-to-date as I see.
There are no config_cs42888.h and wm8960.h files under  ${MY_ANDROID}/vendor/nxpopensource/imx/alsa

instead there are json files where the required parameters are set and the bus0_media_out does not working

0 件の賞賛
返信