i.MX 8M Plus - external eMMC 5.1 connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8M Plus - external eMMC 5.1 connection

1,825件の閲覧回数
Abishek_Devan
Contributor I

Hi Team,

Currently we are working on one of the projects which connect i.MX 8M plus processor connected to external eMMC 5.1. We are planning to improve performance, and we are having some queries,

1. In reference manual the SW_PAD_CTL_PAD_SD1_CLK SW PAD Control Register (3033_02ECh), field 6 (bit 7 - Pull Up / Down Config. Field), if we are changing this field whether it will impact the reference clock to the eMMC 5.1 and it will impact in IP level also?

2. Do you have any uSDHC controller details documents? we are seeing high level block diagram in datasheet, but it has limited details.

Thanks in advance.

Regards,

Abishek

0 件の賞賛
返信
5 返答(返信)

1,714件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Do not have effect, for the usdhc1 you using you can set the same as the usdhc3:

MX8MP_IOMUXC_NAND_WE_B__USDHC3_CLK 0x190

0 件の賞賛
返信

1,792件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Rita_Wang_0-1736845822294.png

 

0 件の賞賛
返信

1,792件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Can the emmc work well ? How about your design for the emmc, are you connect to USDHC1 or USDHC3?

0 件の賞賛
返信

1,783件の閲覧回数
Abishek_Devan
Contributor I

Hi Rita,

Yes, eMMC is working fine. We connected our connection to the USDHC1. 

My question is if we change the SW_PAD_CTL_PAD_SD1_CLK SW PAD Control Register (3033_02ECh), field 6 (bit 7 - Pull Up / Down Config. Field), if we are changing this field whether it will impact the reference clock to the eMMC 5.1 and it will impact in IP level also?

Regards,

Abishek

0 件の賞賛
返信

1,777件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

I will help check it

0 件の賞賛
返信