i.MX 8M Plus Support for USB on Cortex-M7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8M Plus Support for USB on Cortex-M7

1,972件の閲覧回数
cwembedded1
Contributor I

I'm looking for support for interfacing with a USB device from the Cortex-M7 coprocessor of the IMX8Plus.

I am using this SMARC board here from Avnet: https://www.msc-technologies.eu/support/boards/smarc/msc-sm2s-imx8plus.html

Along with this carrier board from Congatec: https://www.congatec.com/us/products/accessories/conga-seval/

From the system running on the A53 processor (Linux) I have access to both USB ports. We would like access to one of the ports from the M7.

Using the SDK SDK_2_10_0_MIMX8ML8xxxKZ I cannot find any USB drivers or examples for this use case. Does this require pin remapping? Does the Cortex-M7 even support IO? Are there other SDKs that contain drivers and middleware that are needed?

Any information or solutions to this along with more information on utilizing the Cortex-M7 would be greatly appreciated.

ラベル(1)
0 件の賞賛
返信
1 返信

1,942件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Yes, there is no driver available for USB available in the official SDK release.

It may be possible to port it from other devices for example i.MXRT, but the PHY and USB non-core registers are different, and it will not be straightforward to port.

Best regards,
Aldo.

0 件の賞賛
返信