i.MX 8M Plus PMIC usage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 8M Plus PMIC usage

1,619 次查看
www1519
Contributor III

Hi! NXP Engineer

In my design, IMX8M Plus+PCA9450C+LPDDR4(refer to NXP EVK) is used.

Now , I want to reduce the working frequency of SOC and LPDDR4,

but the frequencis file is not visible with cat command, can not to be read and edited.

(If use NXP EVK, the frequencis file is visible with cat command, can be to read and edited.)

why is it,   can you tell me?

The difference between my design and the NXP EVK circuit is as follows.

NXP EVK: PCA9450C pin 13(IRQ_B) is connected to SoC pin D6(GPIO1_IO03)

www1519_1-1685278586502.png

 

www1519_0-1685278541178.png

 

My design: PCA9450C pin 13(IRQ_B) w/100k PU is connected to SoC pin AJ16(SAI2_RXC)

Note: The voltage of Soc SAI2 is design with 1.8V and connected to PCA9450C BUCK5. 

www1519_2-1685278711692.png

www1519_3-1685278774688.png

Confirm it please.

Thanks a lot

Best regarads.

 

 

 

0 项奖励
回复
2 回复数

1,446 次查看
www1519
Contributor III

Hi @Dhruvit 

I'm very sorry for the late reply.

the above problem has been solved.

Thank you for support.

Best regard!

0 项奖励
回复

1,563 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @www1519,

I hope you are doing well.

Please make sure that below mentioned options are enabled in kernel options : 

CONFIG_CPU_FREQ=y

CONFIG_ARM_IMX_CPUFREQ_DT=y

Please provide me with debug logs , device tree file and commands used for further debugging.

Please make sure that you have made changes in pinctrl and interrupts property corresponding to IRQ_B pin connection change.

Thanks & Regards,
Dhruvit Vasavada

0 项奖励
回复