i.MX 8M Plus DDR inline ECC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8M Plus DDR inline ECC

1,994件の閲覧回数
Fai1
Contributor I

Hello,

I want to use the ECC feature of LPDDR4 memory with i.MX8MP. To do that, I enabled inline ECC with the i.MX 8 Register Programming Aid (RPA) tool and reflected the changes in lpddr4_timing.c. Then, when generating U-Boot, I set Device Drivers -> i.MX8M DDR controllers->imx8mp inline ECC to Enable in menuconfig.

However, the following message is displayed when booting the Yocto Linux kernel, and the ECC feature is not enabled.

EDAC MC: Ver: 3.0.0
EDAC MC: ECC not enabled
 

Please tell me if there are any missing steps or settings to use the ECC and EDAC features.

0 件の賞賛
返信
1 返信

1,335件の閲覧回数
Rajashekar-Bommideni
Contributor I
Hi, even i have the same issue. Did you find any solution for this ??
Please guide if so
0 件の賞賛
返信