Hi,
I am currently integrating a MIPI CSI-2 solution into our custom hardware. I'm aware of the table in this post https://community.nxp.com/t5/i-MX-Processors/Explenation-for-HS-SETTLE-parameter-in-MIPI-CSI-D-PHY-r... for the HS_SETTLE and CLK_SETTLE parameters, but am unsure if the same is true for i.MX 8M Plus.
Thanks,
Sachin Patel
Hi,
So where can I get those values for iMX8M Plus?
Are they the same as the table above?
Thank you
Hello @igorpadykov ,
we are in the same process here , porting an Ar1335 OnSemi on the I.mx8m Plus.
we have en NDA with nxp and are part of the beta program for the 8mp ,
could we get the same file ? And if any , some files and doc relative to this port ?
my email is visible for you in my account i guess , if not , let me know.
best regard,
Jeremie bours
Hi Jeremie, as NXP support is usually slow to respond, I thought I might as well at least help.
The table in the post I linked for the imx7 board has the same timing parameters, so if for example you want 1000 Mbps/lane, you choose HSSETTLE as 22.
Hi Jeremy, as NXP support is usually slow to respond, I thought I might as well at least help.
The table in the post I linked for the imx7 board has the same timing parameters, so if for example you want 1000 Mbps/lane, you choose HSSETTLE as 22.
A great thank you Sachin !
We used the table accordingly,
we are still stuck with uggly scrambled pixels, but that is the necessary pain when dealing with new camera
400 x 480 RAW10 pixels , recorded in RGBP ( RGB565 ) by the I.MX8M plus :
The pixels seems not well aligned , if you had this kind of behaviour before, do not hesitate !
Best regard, and thank you again,
Jérémie
Hi Sachin
file was sent via mail.
Best regards
igor